Navigation#
Navigate the FactoryTalk Hub Home page using the different controls to provide you the services and tools you want.
You can use the main toolbar to perform these tasks:
Use the Portal Menu to quickly move between the different services included in your organization’s entitlements. This menu also contains hub management tools if you are an owner or admin for the organization.
Click the Rockwell Automation logo to go to the Rockwell Automation website if you want to view additional product information.
The Notifications bell icon alerts you to any new information since the last time you signed on. Click the Notifications icon to review the notifications list and respond to alerts. For more information, see Notifications.
The Help question mark icon provides you with different forms of help. You can review the release notes, getting started information, and help topics. There are also links that you can use to contact support, provide feedback, or view legal information.
Click the Organization name to switch between FactoryTalk Hub organizations. For example, if you are a member of both a system integrator and a solution provider organization.
Click your Profile icon to update Account Settings or Logout of FactoryTalk Hub.
Hub Management Features#
If you are an administrator for your organization you will be able to access Hub Management Features from the Portal Menu. The Hub Management Features are used to create and join organization as well as configure access management, entitlements, user invitations.
Additional information#
If there is a term used in FactoryTalk Hub you aren’t familiar with, check the Glossary for a definition. If FactoryTalk Hub is not operating as expected, contact Support resources.