Processes#

FactoryTalk Remote Access provides a Processes Manager to assist in identifying running processes on remote devices.

Once FactoryTalk Remote Access is connected to a remote device, click Processes to get a list of running processes on the remote system together with CPU usage percentage and Memory Usage. From Processes you can perform the following commands:

  • Stop. Ends the selected process and removes it from active memory.

  • Restart. Restart the remote device.