Connecting to Stratix 4300 Remote Access Router#
Once configured Stratix 4300 Remote Access Router connects to the FactoryTalk Remote Access Cloud Infrastructure and is discoverable by FactoryTalk Remote Access.
To connect to the router, open FactoryTalk Remote Access and click the icon corresponding to the router then click Connect to make the VPN connection to the router.
Then open an https connection to the router IP address and login using your admin user account and password to configure the settings.