Hardware Analysis Details#
The Hardware analysis dashboard provides an overview of the hardware configuration in the project.
The hardware components list includes the following information:
Catalog Number — The Rockwell Automation catalog number of the hardware component
Description — The name of the hardware component
Revision — The firmware associated with the hardware component
Vendor — The original equipment manufacturer of the hardware components
Quantity — A count of the number of these hardware components identified in the project
You can sort and filter the data in this dashboard. If you want to see the information in a different order, you can reorder the columns in the data table by dragging and dropping them as needed. To help you move around the analysis details page quickly, use keyboard shortcuts.