Settings#

The FactoryTalk Remote Access service Settings contains optional settings that are applied to your entire domain.

Customize the domain according to your needs by activating or deactivating the following options:

  • Require a comment when a device connection ends. The system requires the user to insert a comment after a remote connection.

  • Log all connection operations. This option enables the recording of all operation performed on remote devices, categorized by connections. For more information see, Audit.

  • Send email notifications of account information Identifies the email address to which all account notifications will be sent.

Tip

To sent notifications to multiple email addresses separate the email addresses by a semicolon. Example: j.smith@example.com;a.jones@example.com