Stratix 4300 Remote Access Router#
Stratix 4300 Remote Access Router is a hardware device that supports remote assistance services from FactoryTalk Remote Access. Stratix 4300 Remote Access Router can be included in an existing automation network without impacting the plant hardware devices. Adding the Stratix 4300 Remote Access Router does not require modification of the configuration of any of the existing devices.
Stratix 4300 Remote Access Router supports automatic update procedures to provide easy maintenance of the device. Refer to Updating Stratix 4300 Remote Access Router for a detailed description of the procedures.
LED displays on the router provide visual status indicators.
Tip
See the Stratix 4300 Remote Access Routers User Manual (Rockwell Automation Publication # 1783-UM011) for more information on device installation and features.
See these topics for more information about using the router: