Accept an invitation to join an organization#
Invitations to join an existing organization are sent by the owner of the organization. To send you an invitation the owner must send the email to your email address. This email address must be associated with a MyRockwell account. Here is an example of the invitation email:
Item |
Description |
---|---|
1 |
The name of the domain owner who invited you to the organization. |
2 |
The name of the organization you are joining. |
3 |
Connect to FactoryTalk Hub and join the organization. |
Note
If you do not have a MyRockwell Account, you can set it up before attempting to join the organization or you can set up during the join process.
To accept an invitation
Click the Join now button in the email to connect to FactoryTalk Hub and sign in.
An Invitation Accepted Successfully Message displays.
Click OK.