Log details#
The FactoryTalk Remote Access service contains a real-time log of activities on the domain. From this log you can see detailed information, such as:
Which browser was used to open a session with the service
When the service connected to the remote access server
When the server validated the access request
When a transaction started
The amount of packet loss, latency, and jitter in the network communications
When a transaction completed
When authentication succeeds
When authentication fails